STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nucleo MB1364 as standalone ST-Link V3

Hi there,I have developed my project long time with MB1364E, exactly with H723ZG.Now I have got my own PCB with H743. I would like to use ST-Link V3 (SWD) from Nucleo board just the same as it works for cuttable ST-Link from L4 Nucleos, e.g.:https://...

DrDro by Associate III
  • 2860 Views
  • 3 replies
  • 2 kudos

Resolved! SD card error FR_NOT_ENABLED

Hi,I'm trying to send image data to SD card with OV7670 FIFO cam. For the SD card part, I got FR_NOT_ENABLED error all the time. What do I have to do for the error?Also the code:HAL_Delay(200);FIFO_REN_L();FIFO_WE_H();Vsync=0;ov7670_init();res = f_mo...

nucleo-F746 ethrnet, lwip configıration

Hi,I am using Nucleo F746 eval board. I configured ethernet and lwip. But I can't get ping. "Reply from 169.254.255.144: Destination host unreachable." I get feedback like: My ETH and Lwip configurations are below. Can you help with this issue?      ...

HS_1-1695883021586.png HS_2-1695883048330.png HS_3-1695883068608.png HS_4-1695883099184.png
HS by Associate II
  • 3450 Views
  • 8 replies
  • 1 kudos