STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Having issue with STlink_v3minie debugger

Hi all, I am trying to connect to the processor STM32L431CCT6TR via SWD connection, but it says no device found.  Blowe, I have pasted the message and debugger setup information.  It is able to find the debugger. I have also attached the schematic if...

Mehul_0-1701715667541.png
Mehul by Associate
  • 2597 Views
  • 2 replies
  • 0 kudos

STM32G491REI6 got damage

We are using STM32G491REI6. PCB on which this microcontroller has been incorporated, developed by us.In Inverter Application we are using this microcontroller.When it is connected to operate inverter, every time the microcontroller IC got damaged. It...

Resolved! Unable to load to Nucleo board

Scenario:Windows 11 connected to Nucleo-L476RG.Fresh install of STMCubeIDEVersion: 1.14.0Build: 19471_20231121_1200 (UTC)OS: Windows 11, v.10.0, x86_64 / win32Ran STLinkUpgrade 3.13.4Result: Update to Firmware: V2J43M28 STM Debug+Mass storage+VCP Upg...

Dabbo by Associate III
  • 2662 Views
  • 3 replies
  • 1 kudos

Resolved! Exiting from STOP using RTC Alarm A

Hi,Exiting from STOP mode based on RTC Alarm A works nice with ALRAIE (Alarm A interrupt enabled) and ALRAE (Alarm A enabled). Do I understand this mechanism correctly, that I've to have both bits enabled?  Having only ALRAE (Alarm A enabled) isn't e...

Resolved! PCB Design Software for Macbook

Hi Everyone,I would like to know what PCB design software you are using in MacOS for a professional development. Could you give me some suggestions? Because Windows crashes a lot on my laptop and I'm looking for a more stable system. I always use Alt...

Gerald_W by Associate III
  • 3841 Views
  • 2 replies
  • 1 kudos