STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK/V2-1

What is the difference between ST-LINK/V2-1 and V2? Where can I buy v2-1?Or are you buying v2 and updating the firmware?

jinny by Associate
  • 2797 Views
  • 6 replies
  • 1 kudos

Resolved! Missing PG11 on Nucleo UM2581 Board

Hi All,Is there an errata for the STM32L5 Nucleo board?I need to use the SPI on port G which requires PG11 for SPI MOSI.However in the schematic for the board, PG11 is missing from the schematic symbol (see page 3) and there is a gap.  The pin number...

PG11 Missing.png eye1_1-1715799342927.png eye1_0-1715799209577.png
eye1 by Associate II
  • 2398 Views
  • 4 replies
  • 2 kudos

Resolved! DIY ST-LINK V3

Hello.I am creating my own board with an STM32, and would like to also include my own custom ST LINK V3 on the board itself. Is it possible to get your hands on the firmware for ST-LINK V3? I have seen some unofficial attempts, like this: https://hac...

DanielPi by Associate III
  • 14778 Views
  • 10 replies
  • 6 kudos