STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unsufficient disk space on current disk

Hello everyone, i am currently working on STM32 NUCLEO-L073RZ Projects with Ardunio Ide. I did not change anything from yesterday only i install mbed studio and after installation i delete. I did not do anything with mbed just installation,  and i to...

Ekran görüntüsü 2024-05-14 190908.png

mbed touch lcd with stm32h747i-disco

Hello All, My application is quite simple. All I need is a simple LCD touch screen application that can render text and a couple colored squares that has UART comms. When looking at mbed examples for the H747I I found the following from 2019:https://...

gimp3695 by Associate
  • 1188 Views
  • 0 replies
  • 0 kudos

STM32H7B3I-DK: No source available for "<signal handler called>() at 0xfffffffe" while debugging

Hi,I'm attempting to debug the example code (LedToggling) generated from CubeMX, but it's showing an error as described in the image below. The board was working fine before, but suddenly, I'm encountering this issue.      Although I can connect thro...

STM32H7B3I_Debug_issue.png
RLalj.1 by Associate II
  • 1909 Views
  • 2 replies
  • 0 kudos

Resolved! B-CAMS-OMV module connection problem

I want to connect a B-OMV-Cam module to a nucleo board H7A3ZI-Q. When I did my research I found that the only board commonly used with the cam module is the DISCO discovery board. Is the cam module meant for specific bards and if not, how can I conne...

Zeuxis by Associate
  • 2496 Views
  • 3 replies
  • 0 kudos

CC instead of VBUS sensing on STM32G4

I am designing a self-powered device with an STM32G473 and a USB-C connector, and want to be certain about the connections.I have made PCBs with USB-C connectors before, but this is the first time that I have neither a VDDUSB, nor a VBUS Sense input....

EThom.3 by Senior III
  • 2374 Views
  • 2 replies
  • 1 kudos

Resolved! ITM SWO works but i dont know why.

Hello Gentlemen!I have edited this question, former question below just for clarity.New question: the ITM SWO printF-ing works with frequency of 4 MHz. I have searched every little PDF regarding my board (NUCLEO-U575ZI-Q) and i have no clue where you...

Basano_0-1715631555690.png Basano_1-1715630032959.png Basano_2-1715630218932.png Basano_3-1715630284195.png
Basano by Associate II
  • 6615 Views
  • 14 replies
  • 8 kudos

Please recommend a development board

First of all, I want to use the core above STM32F4. I need a few motors, pumps, and sensor control with the MCU.If there are several boards you recommended due to lack of knowledge of hardware, please let me know how to make a physical connection.

jinny by Associate
  • 1678 Views
  • 3 replies
  • 2 kudos