Hi, I have been working with the B-G431-ESC1 for some time.I profiled my motor with ST Profiler and loaded the .JSON file on Workbench and generated the code.My final goal is to be able to control the speed of my motor by sending a PWM signal to the ...
Hi,i am working on STM32F302R8Tx and i would like to have a 490 Hz PWM on Timer15 Channel2, attached are my configuration and my code, when i measure it , i become 491,13..Hz. what can I do to get the exact 490Hz? Any Suggestions?? thank you!!! ...
Hey,i have B-G431B-ESC1 board and Maxon motor. I can not profile this motor. I want to run my motor at 2000rpm max. Speed and 14V voltage source.The MC workbench is able to generate code. I am able to compile and program it using cube IDE. i can con...
ich verwende MCSDK 6.2.0 ich versuche seit einigen Tagen ein Maxon-Motor mit B-G431B-ESC1 zu drehen. aber es gelingt bisher nicht. Könnte jemand mir bitte sagen , was ist falsch eingestellt habe? ich habe mit Workbench alle Parameter von meinem Motor...
Hi @cedric H,Thank you for your feedback.Now the error no longer occurs, it was probably due to my configuration. Now my engine turns without any problems . It's done!!!!
@SRedd.5 thank you for your suggestion.I'm not getting the error message at the moment, but there must be a sure way to resolve this, right ?I still can't profile the engine. Do you have a suggestion? best regards
Hello Gaël A ,thanks for your feedback.I have made several attempts so far and this is my observation. I hope you can give me more tips to make my motor 100% well controlled.1) I tried profiling the motor but that didn't work, the motor just makes so...
Hallo @cedric H ,first of all, thanks for the quick feedback. i'm trying to create the motor profile right now, but this is the error message i'm getting in the attachment. do you have any other suggestion for me?