cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5A9J-DK ITM

IVent.1
Senior

Hallo,

is there something I have to check if ITM_SendChar doesn't work? I mean, I have overwritten the write function in syscalls.c and enabled in the debugger settings the swv viewer at the correct clock, enabled swv trace (the same things I did using the nucleo board), but nothing appears in the ITM Data  Console. Is there something else to configure?Now I'm using this board. STM32U5A9J-DK

Thank you

Isabella

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
boxtor
Associate II

If I remember right, you need to move solder bridges to get the SWO output to work.  See SB33 and SB34 in the manual and the section "SWD debug/program/trace and JTAG/USART".

View solution in original post

1 REPLY 1
boxtor
Associate II

If I remember right, you need to move solder bridges to get the SWO output to work.  See SB33 and SB34 in the manual and the section "SWD debug/program/trace and JTAG/USART".