STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Nucleo support for 1.8V

Hi I'm using the STM32H755ZI board which has the option for 1.8V DVDD (using JP5). Does switching DVDD to 1.8V from 3.3V limit the functionality of the board in any way ? Are the interfaces (CAN, I2C, SPI, UART etc) still functional at 1.8V ?  Thank...

smul by Associate
  • 1145 Views
  • 1 replies
  • 0 kudos

STM32G031K8 Nucleo Error in RAM

HiWe've got here 3 STM32G031K8 Nucleo. 2 of them had problems with RAM access. 1 works fine at the moment.For example STM32CubeProgrammer shows by RAM DumpKeil shows STLink Utilities hangs by Access of some RAM address. Is this a known Problem?Is the...

Prog.png keil.png
CanRF by Associate III
  • 1514 Views
  • 2 replies
  • 0 kudos

STM32F072 USB Connection

Hello everyone!I have a problem regarding my STM32F072 MCU board that I designed: I cannot connect the board with a terminal properly. Let me explain:1. I've managed the program the board using ST-LINK V2 (Chinese version) and SWD pins.2. When I conn...

AlexB99 by Associate II
  • 2099 Views
  • 1 replies
  • 0 kudos