STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F7x2 vcap1 - looking for compatible capacitor

According to AN4661 "Getting started with STM32F7 Series MCU hardware development ":"When the voltage regulator is enabled, VCAP1 and VCAP2 pins must be connected to 2*2.2 μF low ESR < 2 Ω ceramic capacitor. In the STM32F7x2Rx devices, only the VCAP1...

0690X00000A9ovFQAR.png
RBoer by Associate II
  • 1021 Views
  • 0 replies
  • 1 kudos

Set Read Out Protection (Level1) in STM32F446

Hi folks,I am trying to set the RDP option bytes to have my code in flash read-protected. Instead of using ST-Link Utility, I want to set the read-out protection in the code itself (specifically, inside a self-designed bootloader). For this purpose, ...

JSaez by Associate II
  • 4313 Views
  • 4 replies
  • 0 kudos

Resolved! Need Evaluation Kit for this controller STM32L452RCT6 . Is there any alternate Eval Board available?

Actually In our Company the Controller is using STM32L452RCT6 Before Getting A sample Design Board. I need to test with any Eval Board of STM32L4 Series. I Need Evaluation Kit for this controller STM32L4RCT6 Is there any alternate Eval Board availabl...

Lucky by Associate II
  • 4706 Views
  • 11 replies
  • 0 kudos

STM32G431KBT6 SHort-Circuit on VDDA

I made two projects using the new 36-pin STM32G431KBT. In both projects, after a few seconds of 3.2 Volt power supply, the VDDA pin is short-circuited with the VSS / VSSA pin definitively. As many as 5 chips broke this way. Is it a manufacturing defe...

elb-lab by Associate II
  • 1024 Views
  • 1 replies
  • 1 kudos

DB1M for STM32L4R5QGI6

Hi,We have a question about DB1M of STM32L4R5QGI6. According the the user manual, The DB1M should be enabled. Why does the DB1M be disabled on version 4.5? and be enabled on 4.2? Could you help to check it? Thank you.

JHsu.14 by Associate II
  • 1709 Views
  • 1 replies
  • 0 kudos

Unable to ST-LINK Utillity to G0

Using STM32 ST-LINK Utility v4.2.0.0, STLinkUSBDriver.dll v5.0.3.0, ST-LINK_CLI.exe v3.2.0.0, ST-LINK/V2 with firmware V2.J34.S7 STM32+STM8 Debugger I am able to connect to a STM32G0 (Device ID 0x460, Rev B).Using STM32 ST-LINK Utility v4.5.0.0, STLi...

DWrig.32 by Associate
  • 1107 Views
  • 0 replies
  • 0 kudos