Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I need to read/write data into the external Serial NOR Flash (MX25U25645GMI00) via Quad SPI of STM32L412RB board using STM32CubeIDE.I was able to get the Device ID of the MX25U25645GMI00.I am unable to write/read data into the MX25U25645GMI0 in Auto ...
Hi Team,I'm using STM32 USB CDC FS on my custom board. In the Windows Device Manager, it shows as "STMicroelectronics Virtual COM Port (COM6)." I want to change it to display a custom name for my board. Here are my questions:How can I change the devi...
I accidentally disabled the 3v3 pin on CN8, so now my Nucleo h755 board can no longer load the code.In this case is there a way to save?Thanks,
Hello team,I’m working with an STM32H745iik6/ Nucleo-H745ziq microcontroller and currently using USB DFU mode to upload firmware. The process involves setting BOOT0 to 1 and performing a manual reset to enter DFU mode. After uploading the new firmwar...
I am used the board for 4hrs single Strech.Used the proper ST Link debugger.Console Message:Target no device foundError in initializing ST-LINK device.Reason: No device found on target.
hello. My name is Kim and I work for a company in Korea. I have been trying to purchase ST-LINK/V2 products from STMicroelectronics Korea, but I have not been able to get in touch with them. I contacted the STMicroelectronics Korea distributor, b...
Hi,I am working on a project to control BLDC motor so I configured the TIM1 as shown below:I have selected the TGRO trigger event selection to be "Update Event". I have confusion now because when the counter mode is "Center Aligned Mode 3" the update...
Hello I am trying to move a small io project to smaller chip. I am trying no code project just confirm enter debugger works.STM32F103C8T6 STM32Cube IDE 1.9I Get ST-Link Error When attempting to debug. Reason(18) Could not verify ST device! Abort conn...
Hii everyone,I want to debug STM32F103C8T6 controller by using the debugger present in the STM32F446RE nucleo board. After setting the parameters , when i go for debugging the following error is coming. Please guide me how i could debug my respective...