cancel
Showing results for 
Search instead for 
Did you mean: 

I recently bought NUCLEO-G474RE and found a problem.

aarom
Associate II

The problem is pin PB4, which is always powered.

It is the same as returning to "STM32CubeG4_Demo_NUCLEO-G474RE.hex".

Do I need to send it in for repair??

How to send??

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @aarom and welcome to the ST Community :smiling_face_with_smiling_eyes:.

The PB4 is internally pulled up after Reset.as you can see on the page 72 of DS12288 Rev 6:

"After reset, these pins are configured as JTAG/SW debug alternate functions, and the internal pull-up on PA15, PA13, PB4 pins and the internal pull-down on PA14 pin are activated."

So, this is normal.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @aarom and welcome to the ST Community :smiling_face_with_smiling_eyes:.

The PB4 is internally pulled up after Reset.as you can see on the page 72 of DS12288 Rev 6:

"After reset, these pins are configured as JTAG/SW debug alternate functions, and the internal pull-up on PA15, PA13, PB4 pins and the internal pull-down on PA14 pin are activated."

So, this is normal.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

aarom
Associate II

Other functions are currently normal!
It would be better if the pins could be arranged in order!
I can only update the definition using *.h,
Thanks for your reply.