STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK error after mass erase

Hi there,I want to write a bat file to program STM32 MCU.After I issue the command below to erase the full chip.STM32_Programmer_CLI.exe -c port=SWD freq=4000 -e allThe prompt says: 'Mass erase successfully achieved', which indicates the full chip er...

Spencer_Y_0-1720060225224.png
Spencer_Y by Associate II
  • 2275 Views
  • 3 replies
  • 0 kudos

NUCLEO-L433RC-P SWV Not Working

Hi,I have an external PCB using STM32L432KCU6 to program and debug.  I can program this using the NUCLEO-L433RC-P (MB1319C) and NUCLEO-L476RG development boards in STLink configuration.Using the L476, I can see the output of the SWV from printf (MCU ...

jdawkins by Associate II
  • 3681 Views
  • 7 replies
  • 1 kudos

Resolved! Target unknown error 19

I am using STMCubeIDE v1.7 on MacOS 10.15.7 and connecting to my target via an STLINK V3. I updated CubeIDE to v1.7 and it suggested an update to the STLINK. Since doing that update I am not able to connect to my target (STM32F405). Errors given a...

RWebb.1 by Associate II
  • 10087 Views
  • 7 replies
  • 0 kudos

nucleo pd output 24V@3A

Can I safely get that power out of any of the nucleo PD boards with a usb3 pd input? Can I get any higher current or voltage?  Output is 2 pin barrel connector. Target application is fully documented here. Thanks so much in advance Joe