STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error in final launch sequence

 Hello,I am attempting to run a p2pServer_Ext sample application on my Nucleo WBA52CG board. Currently, I have a heart rate sensor application running on the same board. However, when I try to flash the new p2pServer_Ext application, I encounter an e...

Hardik02 by Associate II
  • 6390 Views
  • 6 replies
  • 2 kudos

I2C Slave RX callback doesn't called

Hello everyoneI am using NUCLEO-H563ZI as master I2C, and STM32F412G-DISCO board as slave I2C, which should mimic temperature sensor TMP117.I am trying to send from master to slave a register number to read from, but the rx callback in the slave does...

MichaelR_0-1721544888128.png MichaelR_1-1721545083709.png
MichaelR by Associate III
  • 1687 Views
  • 2 replies
  • 0 kudos

Resolved! using LCD-TFT controller without HAL

Hello, i am trying to configure the on-board TFT-LCD on STM32F429-Disc0 board and i want to do it without using HAL drivers, every tutorial on youtube or other platforms i see, are using CubeMX or HAL or both. I understand we need SPI5 to configure t...

sk12 by Associate II
  • 7335 Views
  • 11 replies
  • 8 kudos

STLink V3-PWR and OpenOCD

Are there plans to add support for the STLink V3-PWR to OpenOCD?  At present, the USB device interface appears not to be supported (using the latest openocd snapshot).  STLink V3-MINIE works fine with openocd. For the V3-PWR, see the error (boldface ...

DAlbe.3 by Senior II
  • 8138 Views
  • 5 replies
  • 1 kudos

Resolved! UART on F7508-DK

I am trying to implement a data transfer using UART on the STM32F7508-DK, but cannot get it to work. I have been trying for the minimal example from the step-by-step instructions https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Step3_Introduction_to...

Jamiw by Associate II
  • 1496 Views
  • 1 replies
  • 1 kudos