User Activity

Hello, I think there's a bug in CubeIDE when working with a Nucleo-H563ZI. Steps to reproduce it:- create new project, clear pinouts- enable USART3 in async mode, PB10 and PC4 pins are assigned (why not PD8 and PD9? don't understand)- ctrl+click on P...
Hello,I would like to know if Nucleo-H563ZI board could be used as a USB host, using the user USB (CN13). I'm asking because I'm a bit confused, honestly - I've only found examples where it's being used as a device and the board manual seems to menti...
Hello,Just got a new Nucleo-H563ZI board and I was trying to connect it to PC through the STLINK USB-C port, in order to play with it. I've checked jumper config, and all seems right, but the only thing happening when plugging in is that LD4 RED half...
Kudos given to