STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-IDB00BV2

All:I have the IDB00BV2 and am using the Keil Uvision_5 tool with the compiler back leveled to version V5. I'm using this board to test software to be run on the BlueMRG-2 running on my product. I have the ST BlueNRG-1_2 DB32.3 Project software insta...

KBloo.1 by Associate
  • 814 Views
  • 0 replies
  • 0 kudos

STM32 Nucleo-F767ZI no ping IP

STM32 Nucleo-F767ZI no ping IPWhen I build project no errorI configured static IP And HTTPD enabledI added next lines#include "lwip/apps/httpd.h" httpd_init(); while (1){MX_LWIP_Process();/* USER CODE END WHILE */ /* USER CODE BEGIN 3 */}/* USER CODE...

shef777 by Associate II
  • 3437 Views
  • 5 replies
  • 0 kudos

Resolved! Did I broke my STM32?

Hello together,I just tried to get my STM32F407-Discovery working. I wanted to upload the firmware by putting it into DFU Mode, connecting it via USB to my computer and using CubeProgrammer to upload the code into the STM32s memory. So I connected BO...

need help for smbus communication

hi i have asked this few times but its unclear to me how i am supposed to communicate between the host and slave device over smbus protocol. do we have a detailed documentaion which includes which needs to be enablesd 0n the baord for the communicati...

_kalpesh by Associate III
  • 1096 Views
  • 1 replies
  • 0 kudos

Bare metal programming issue

I am a beginner in embedded programming and I have a problem programming the nucleo board. I want to turn on the LED built into the board and connected to the PA5 in a bare metal way, but I could not turn it on even though I followed the steps that I...

ALMAAROUF_0-1723744937707.png ALMAAROUF_1-1723745002780.png ALMAAROUF_2-1723745080558.png ALMAAROUF_3-1723745127137.png
ALMAAROUF by Associate II
  • 1823 Views
  • 2 replies
  • 2 kudos