Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello,I’m not sure that is this important, but the board I’m using is the STM32F413ZH. When I try running an application on the STM32, it generally works fine, but sometimes after exiting debug mode, it stops working. Actually, this isn't a big probl...
When I connect to my computer with a USB connection to upload the code to the nucleo-f446re board, that part of the board gets very hot. I didn't forget to jump to the U5V all the time when I connected to the computer with the USB. Why does this happ...
Hi, what is the difference between .elf file and .bin file to program STM32. If I load up the .bin file and program STM32, will it contain all the necessary such as program data and flash data. Is there a application to program individually the .bin ...
Hello can anyone please help me with the SWD pin status. What can be the expectation?
Hi,I have Nucleo-H743ZI2 and Nucleo-U575-Q boards.I can see that we can upgrade the st-link firmware for STM32 boards via STM32CubeProgrammer, ST-LINK Utility or STSW-Link007 tool. But I have observed that this will always pick up the latest version ...
Hello, I am following this application note an5496-guidelines-for-the-buck-voltage-mode-on-the-bg474edpow1-discovery-kit-stmicroelectronics-1.pdf for the B-G474E-DPOW evaluation board. My problem is I can not change the load bank using the joystick n...
Hi everyone,I am trying to run an ethernet phy (LAN8742Ai) using STM32H745. I can say that there is no major difference from the Nucleo ref. phy design. However, when i ping, i cannot get a response and the processor gets very hot. The phy and MCU bl...
STM32H750 Discovery Kit board, Timer 1, Ch1 (PA8 output) I used direct access to timer registers as a HAL library and the result was similar. I can receive 10 MHz with direct access to register and TIM1->PSC = 10; But when I set TIM1->PSC = 1 I do...
hello NXP Expert, I am trying to achieve the maximum speed for the ST7735S 1.8 inch TFT, but it's very slow on the STM32 microcontroller. However, it reaches maximum speed with the NXP controller. In the video below, you can...
Hello, I need a to find a Nucleo board with 2 12-bit ADCs and at least 2.4 MHz sampling frequency. I also need an integrated external phy for HS usb2.0 data transfer. Which STM32 boards are in correspondence with these requirements? Thanks in advance...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.