2024-04-12 5:30 PM
Hello. I have a Nucleo-G474 and I want to bypass the onboard STLINK-V3 programmer and use an external programmer module (STLINK-V3MODS). I have the proper connectors and ribbon cables to connect to the MIP10 connectors.
The program sees that the device does have 3.3 volts and it does see the STLINK-V3MODS module. However it does not see the target. Below is the message.
I've tried all sorts of things, like moving jumpers around to disable the onboard ST-Link. I removed some of the 47 ohm resistors that could interfere with the external programmer. I can't find any information on how to use an external programmer with the Nucelo-G474 board.
The reason for this exercise is that I am not going to use an onboard ST-Link programmer in my application. I need to use an external programmer and I want to ensure that I have a working design to do this with.
Thank you, Richard V
Message from STM32CubeIDE:
STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
2024-04-16 2:04 AM
Hello,
I think it should work without removing any 47ohms resistors, only JP1 should be closed to keep the onboard ST-Link at a reset state.
Just to be sure this is not a STM32CubeIDE settings problem, maybe you could try to connect with the STM32CubeProgrammer ?
As long as at least the SWDIO / SWDCK / T_VCC / GND pins are connected, I think that should work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.