User Activity

Hello Everyone, For a project, I'm using a NUCLEO-L432KC board and it is connected to external sensors, Tx, and Rx (which work with 4-5 V). I want to use an X-Nucleo-LPM01A to measure its power consumption. Based on the NUCLEO-L432KC documents, I hav...
In my application, I receive a message from LoRa and intend to transmit it via UART1 which is set to PA9 and PA10. However, when I check the UART RX using a logic analyzer, I do not receive anything.I have tested the UART1 alone in a simple project, ...
Kudos given to