STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about UART communication

Hello everyone,I am using the b-g4743-dpow1 discovery kit and I am trying to perform UART communication. However, the board does not output the UAR output to the computer. Currently, I can read the observe the UART output through oscilloscope, the ou...

OFN by Associate II
  • 1714 Views
  • 3 replies
  • 0 kudos

Resolved! GDB server

What should I do when stm32 applications do not see st-link and the message I always receive is: Failed to start GDB serverFailed to start GDB serverError in initializing ST-LINK device.Reason: (2) ST-LINK DLL error.No matter which stm32 board or cab...

zom by Associate II
  • 3390 Views
  • 5 replies
  • 2 kudos

Library Compatibility

Sorry if formatting is trash this is the first post on the forum. Our lab group is trying to get I2C connectivity to a external chip using an I2C. The problem that we are having is getting the clock up and running. We downloaded both the L4 and F4 pa...