STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5G7VJT6Q power section

Hi,We are currently working on a design involving the STM32U5G7VJT6Q microcontroller and would appreciate your expertise in reviewing the power section of our design. I have attached a diagram of the power section for your reference.Could you please ...

NIVI_1-1724646874948.png
NIVI by Associate III
  • 1088 Views
  • 0 replies
  • 0 kudos

Resolved! ST-LINK source code

Hello Currently i'm using STM32F769I-EVAL board with on-board debug unit ST-LINK/V2-1. I would like to know whether ST-LINK/V2-1 firmware is open source & freely available for end user ?Could someone hint ? Thanks. RegardsBivin

NUCLEO-H723ZG (ADC DMA TIM2 LWIP UDP)

  I am doing research to test the performance of an MCU based system that transports the raw PCM samples of the STM32H723ZG ADC via Ethernet, LWIP in UDP.the ADC is set to 8 bits of single resolution, and I have set the TIM2 timer to drive the ADC cl...

AntoR by Associate III
  • 987 Views
  • 0 replies
  • 0 kudos

STM32H723 serial communication using USB

Hi,I'm trying to build a small board using the STM32H723 MCU and my requirement is that I have one USB Micro B receptacle on the board for communication with the MCU. However, the communication should happen via USART and not the standard USB protoco...

smn by Associate
  • 3242 Views
  • 3 replies
  • 0 kudos