Hello I have been using an STLink v3 pod successfully for several months but suddenly it stopped working. The green light is lit and the red one flashes slowly. I cannot see it in Device Manager and there are no Unknown Devices. There is no chime...
The pod isn't dead. It works fine if I plug it into a different compuer.I would be perfectly happy if I could just use a different ST Link V3 pod but it does the same thing when plugged into my computer. I suspect it's a driver issue but I don't kno...
I got this response from ST: "I'm confirming that this 220pF is indeed required for designs using LQFP/BGA packages as shown per table 2 in the forum post. I can see from an end customer's POV how this could be confusing as in Figure 2 there's no ex...