STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

sm32h7 firmware only running after reset

hi guys ,  I have been working on a stm32 project like a digital automotive cluster using STM32H7A3ViT6 MCU . I am using the LTDC module to drive the display . now the problem is the mcu dosent run the code on powerup but it ll do when i press the re...

Capture.PNG
b1aze by Associate III
  • 230 Views
  • 2 replies
  • 0 kudos

Resolved! USB CDC on Nucleo-G431RB-C04

Hello,I would like to build up an USB-CDC communication which gets the commands from the PC and forwards the messages to CAN. I have choosen a Nucleo-G431RB-C04 board, which have a FDCAN and a USB-FullSpeed inteface also. Do I able to create an USB-C...

PecasHUN by Associate II
  • 369 Views
  • 7 replies
  • 1 kudos

B-CAMS-OMV Alternative

Is there any alternative of "B-CAMS-OMV" to use with "STM32F746G-DISCOVERY" as in my region it is not available and the cost will be huge if I want to ship it to Bangladesh. So, is there any alternative modules that I can search for?

alaraf by Associate
  • 155 Views
  • 2 replies
  • 1 kudos