Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Dear all,I'm unable to connect via SWD to my STM32F103C8T6. What ever I try I get no target found with STM32CubeProgrammer or ST-LINK Utility (I have tried all combinations at slow and high speeds). - device is virgin- BOOT0 is low- NRST unconnected ...
Hello everyone, I’m facing an issue while trying to debug my project custom_for_stm32f103c8t6 in STM32CubeIDE. When I launch the debug session, I get the following error message: Error in final launch sequence:Failed to start GDB server What I’ve t...
Hi, I tried to configure the USB Host for a project, but it’s difficult to configure, and I am not finding any online support available for the STM32H5 series controller.My requirement: I configured PB4 as an output, which is connected to a green LED...
I have a NUCLEO-F103RB (MB1136 rev C05). My goal is to remove the ST-LINK and power via a hat supplying 3.3v. For the 3.3v I have: Moved JP5 to pins 2-3.Checked JP1 is removed.Removed SB2 zero ohm resistor.Removed SB12 zero ohm resistor.Verified my s...
Hello, I’m having a problem with a board I’m developing based on the STM32H747BIT6. The issue is related to SPI communication. When I connect any device to the SPI bus, the signal level drops from 3.3 V to around 1.5 V. I have tested different SPI pe...
Hi all, I have a small issue with the STM32N6570-DK board and the VENC_SDCard example code. The PN12 pin has a voltage of 0V (card inserted) or 1.80V (no card inserted); on the MCU side, the GPION data register (IDR) always shows a logic 0 in both si...
Hello ST Community,My name is Gorakhnath. I am currently pursuing M.Tech (Power Electronics and Drives) at NIT Kurukshetra. I am using the STM32F4DISCOVERY (STM32F407VGT) board and I need stable DAC outputs for my hardware application.What I need (re...
Hello,I got a radio MCU which connects to cloud and can receive binaries from database. And I got a STM32 that controls some stuff, including other MCUs. In production this means a lot of headers and programming time for all of them, no way to update...
Hi, I’m using a NUCLEO-144 (STM32H563ZIT6) development board with only the board USB STLINK-V3EC port connected. TRACE and DEBUG are enabled with Serial Wire in the configuration file, and printf is routed through ITM: int _write(int file, char *ptr,...
When will the NUCLEO-C5A3ZG be available via distributors?The st.com site lists it as available(mass production), but none of the distributors has listed it at all. And the estore lists it as coming soon. Do you have any more concrete dates, will it...