STM32 MCUs TouchGFX and GUI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H745, Use of TouchGFX, Ethernet and LwIP

I am currently working on a project using TouchGFX, Ethernet an LwIP on a STM32H745I board and I was wondering if anyone has encountered a similar issue.I am using :the firmware package v1.9 for the H7 (I also tried with the v1.10),TouchGFX 4.18 (I a...

0693W00000QKwdtQAD.png
QRobe.1 by Associate II
  • 821 Views
  • 5 replies
  • 1 kudos

STM32H750 JPEG: Video processing is always stuck

In my project, SD card was used to store the video, JPEG peripherals +DMA2D were used to convert the video format and finally displayed on the LCD screen, but only the first 4 frames could be converted each time, and then HAL_JPEG_DecodeCpltCallback ...

MaChao by Associate II
  • 243 Views
  • 1 replies
  • 0 kudos

Resolved! Textearea glitches (touchgfx)

Hello,I'm currently developing an application on a STM32H753VT6 with touchGFX and I have an issue with textAreas. Just to say that I'm using my personnal font ( size : 20/24/34 px). Each textArea has just one wildcard with a 17 chars size buffer. I'm...

0693W0000059ikzQAA.jpg 0693W0000059ilFQAQ.jpg 0693W0000059ij9QAA.jpg
AJT141 by Associate III
  • 651 Views
  • 4 replies
  • 0 kudos

I have a problem with a Riverdi 10.1 display.

Hello, I hope you are well.The problem is, I create a project in TouchGFX Riverdi_101STM32H7 v2.2.0 (to get the BSP folder), I generate the code in TouchGFX, then I open the STM32CubeIDE, I compile with STM32CubeIDE and I don't have any error. I try ...

FGuti.1 by Associate II
  • 640 Views
  • 4 replies
  • 0 kudos

TouchGFX 4.21.0 rendering problem

since i Updated to TouchGFX 4.21.0 (from 4.20.0) the LCD shows a visual artifactit happens when rendering images in the L8_565 format (plain RBG_565 works) or texti'm using a STM32 nucleo board with a STM32H7A3 processorwhen i generated the code with...

0693W00000Y85hHQAR.jpg 0693W00000Y85hvQAB.jpg
CRich.4 by Associate III
  • 1792 Views
  • 13 replies
  • 3 kudos

Resolved! External loader fails to download

Hi all,I'm trying to put some TouchGFX data (images, text, ...) in an external flash (S25FL128L) on a custom board with STM32H7B0VB mcu. I'm using the octo-spi peripheral as quad-spi.So, I follow the guide to make an external loader and I did it. It ...

nikof by Associate II
  • 4546 Views
  • 21 replies
  • 1 kudos