User Activity

I have a motor control board built around the STM32F446RET6. I was updating code using motor control workbench to alter the control parameters.After an update, I was no longer able to use the motor control workbench console to communicate with the bo...
In my application, I am driving a low voltage, low speed PMSM with a custom power electronics board. Using motor control workbench, I have a configuration where I can reliably start the motor and it spins up to speed.However, the reported speed thoru...
I am working with a custom SM-PMSM, and built a motor drive to power it.The motor does not start, and the START-UP FAILURE always occurs. There is a pulse of current delivered to the motor, which I assume is used to orient the rotor.Using the monitor...