STM32 MCUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! no Satel-VL53L8CX SPI example

Hi! I am developing a project which uses the satel-Vl53l8cx. I found many examples in I2C but none in SPI.The only one would be in VL53L8CX_ULD_driver_2.0.0 but this one was coded for the X-nucleo-Vl53l8A1.   A wiring is shown in AN5945 in SPI but in...

Antonin_m84_5-1720044853550.png Antonin_m84_6-1720044872426.png

Possible shortcoming in HAL SD library

Been trying to get an test application working on a STM32F469NIH Discovery board.Should be fairly simple - Write a file to the SD Card, with FatFS, the read back:Try as I might, I couldn't get things working.After a bit of debugging, I think the issu...

MClar.3 by Associate II
  • 738 Views
  • 3 replies
  • 0 kudos
Labels