STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Question about the STM32F429 board

Hi, I'm having some problems with the STM32F429 DAC testing. I have two boards of the same type. On board 1, the Digital Storage Oscilloscope shows that the sine wave voltage ranges from 2.08V to 2.94V. However, on board 2, with the same program and ...

S__46260271_0.jpg S__46260273_0.jpg
tasabao by Associate
  • 340 Views
  • 4 replies
  • 3 kudos

Is my NUCLEO-F401RE board damaged?

After using the board for a couple of days, the board started giving the following error is Keil-MDK:And the two led's (LD1 & LD3) are always RED as shown below:And the Nucleo USB drivers are installed: I tried also to put the chip into loader mode (...

SamSamuels_0-1722535229229.png SamSamuels_1-1722535323107.png SamSamuels_3-1722535518200.png SamSamuels_4-1722535879278.png

How to use X-NUCLEO-GFX02Z1 board

Hi all, I just bough this display extension board GFX02Z1 and have a Nucleo-F412ZG. I tried to follow the ST tutorial to write hello world on the display, but I ran into some issues. And being completely new to CubeIDE, I have no idea what's going on...

YordanEng_0-1721725207272.png YordanEng_1-1721725254735.png YordanEng_2-1721725475673.png

Resolved! STM32F030F4P6 using UART

I have a custom PCB I designed where I intend to use UART via PuTTy, however, I'm not entirely sure how to do this through the cube IDE. Normally with the Nucleo L476RG, the device is recognized and I upload code via USB, however, I need to flash the...

DRicc2_0-1722128603925.png
DRicc.2 by Associate III
  • 264 Views
  • 3 replies
  • 1 kudos

I2C Slave RX callback doesn't called

Hello everyoneI am using NUCLEO-H563ZI as master I2C, and STM32F412G-DISCO board as slave I2C, which should mimic temperature sensor TMP117.I am trying to send from master to slave a register number to read from, but the rx callback in the slave does...

MichaelR_0-1721544888128.png MichaelR_1-1721545083709.png
MichaelR by Associate III
  • 234 Views
  • 2 replies
  • 0 kudos

using LCD-TFT controller without HAL

Hello, i am trying to configure the on-board TFT-LCD on STM32F429-Disc0 board and i want to do it without using HAL drivers, every tutorial on youtube or other platforms i see, are using CubeMX or HAL or both. I understand we need SPI5 to configure t...

sk12 by Associate II
  • 724 Views
  • 11 replies
  • 8 kudos