Availability of CANOPEN Stack
Hi, If there is any CANOPEN Master Stack/library available for STM32 controller, please share all those references with integration steps. Thanks,Parth
Hi, If there is any CANOPEN Master Stack/library available for STM32 controller, please share all those references with integration steps. Thanks,Parth
All:I have the IDB00BV2 and am using the Keil Uvision_5 tool with the compiler back leveled to version V5. I'm using this board to test software to be run on the BlueMRG-2 running on my product. I have the ST BlueNRG-1_2 DB32.3 Project software insta...
Hello,I have a custom made board, currently running with just an STM32F030K6T and a simple regulator on it.Trying to implement power saving modes I face some weird behavior on the DBG module of the MCU.The problem is that even after writing the DBG_M...
Hello everybody, I am somewhat new to the world of STM and still learning. I have written the code that reads the data over UART than it sends specific data "calculated" from the UARTS data to SPI then it reads back from SPI than it sends it to UART....
Hello everyone!I have a problem regarding my STM32F072 MCU board that I designed: I cannot connect the board with a terminal properly. Let me explain:1. I've managed the program the board using ST-LINK V2 (Chinese version) and SWD pins.2. When I conn...
Hi,I am looking for a SD Card image from STM32F072B-EVAL kit. Without it demo program can not run. Package from ST site (en.stsw-stm32137) contains files from SD card, but it seems it does not work. I will be grateful for help.
Hi, For some time now I was using cheap bluepill and stm32f030-demo boards to debun my project with st-link probes. It all works perfect. But recently the stmf030 become too small, so I decided to replace it with stm32f070 (same tssop20 package as or...
Hi everyone,I'm a beginner in electronics design but I'd like to create my own PCB.I've designed a schematic around the STM32F0 microcontroller and would greatly appreciate any feedback you might have.The setup involves a board with one transmitter a...
When I hit Debug. System stops at first line of main() as intended. However no matter how I setup any breakpoints on the rest code, and hit Resume(F8) button. The code never stops on those breakpoint. even though I am 100% sure those breakpointed li...
Hello,I am working on a project where we have a main board and a header board connected via SPI. We have the ability to update the firmware of the main board over the air but not for the header board. We now have a need to update the firmware of the ...