cancel
Showing results for 
Search instead for 
Did you mean: 

Eval Board ADXL354

fru999
Associate III

Hey everyone, 
I am working with the ADXL 354 eval board with an STM32H745

data sheet ADXL354 : https://www.analog.com/media/en/technical-documentation/data-sheets/adxl354_adxl355.pdf

data sheet eval boad: https://www.analog.com/media/en/technical-documentation/user-guides/EVAL-ADXL354-355-UG-1030.pdf

 

I have configured the pin PA0-C for the ADC. 

I have connected all the pin as indicate in the datasheet (exept the VDDIO and GND of the RANGE and Mode because if i do so, the thing is not working at all) but the output is always the maximum (if my ADC is configured as 8 bit, the accelerometer returns 255)

If I move nothing change. So I connected the GND of MODE and RANGE and I have value (again if I connect the VDDIO of RANGE and MODE, it is not working at all) but my acceleremeter become really really hot (not brun but...)

 

Can you help me with that ? 

Thanks ;)

1 REPLY 1
Andrew Neil
Super User

Please post a schematic (aka "circuit diagram")  - it's a far more effective way to show connections than trying to use text!

Some good, clear photos may also help.

 


@fru999 wrote:

I have configured the pin PA0-C for the ADC. 


How have you configured them? Please give full details.

 


@fru999 wrote:

I have connected all the pin as indicate in the datasheet (exept the VDDIO ;)


Are you sure that's valid?

VDDIO is the supply for the digital interface - so it won't be able to communicate without it.

You should confirm this with Analog Devices - support links on their Product Page:

https://www.analog.com/en/products/adxl354.html

 


@fru999 wrote:

but the output is always the maximum (if my ADC is configured as 8 bit, the accelerometer returns 255);)


Is that because the ADXL354 is actually outputting "maximum", or is it because your STM32 is not correctly reading the value?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.