STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PCB and Schematics for NUCLEO-H563ZI

Hi I am designing a PCB using STM32H563ZI. Can you share the project files for NUCLEO-H563ZI ? I am using Altium Designer. If the files are in different format, I can import them to Altium. I have shared the link and the name of the evaluation board ...

STM32F072B-EVAL SD card image

Hi,I am looking for a SD Card image from STM32F072B-EVAL kit. Without it demo program can not run. Package from ST site (en.stsw-stm32137) contains files from SD card, but it seems it does not work. I will be grateful for help.

pawelr by Associate
  • 207 Views
  • 1 replies
  • 0 kudos

Resolved! NUCLEO-H7S3L8 Schematics

Hi all,I am using the NUCLEO-H7S3L8 board, and I looked for the schematic or wiring diagram for this board in the ST website, but I couldn't find it. Anyone knows where that information may be available. Thanks,Amilton

RS485 Sensor

Hi, I am trying to connect one energy meter sensor which has RS485 output , But i am unable to read RS485 sensor readings in Nucleo F401RE, If you have any examples please help out!!

Resolved! Error in Nucleo-U031R8 SCK Connection

I fear there is an error in the new Nucleo-U031R8 board. The D13 pin is labeled as the SPI1 SCK pin on the boards' silkscreen. However, the board schematic shows that this is connected to PA5. STM32CubeMX reports pin PA1 as the actual SPI1 SCK pin.So...

JSGraaf_0-1713917280613.png JSGraaf_0-1713917709786.png
JSGraaf by Associate
  • 404 Views
  • 2 replies
  • 1 kudos

STM32 l432KC USART2 serial debug

I am trying to communicate(Tx and Rx) with the arduino serial monitor using USART2 using ppins PA2 and PA3 respectively. This si done with the assumption that these are the pins which are connected to the USB serial wires. Mt USART Tx fucntion is wor...

Using RC522 module on STM32F401

Hello,For a school project, I am trying to use the module RC522 module to do RFID tagging with a Nucleo F401RE. I had some issues to do it and was wondering if anyone has a good library with this board.If needed, I can provide you my code.

Hippo by Associate
  • 795 Views
  • 3 replies
  • 0 kudos