STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1081 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4105 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 8145 Views
  • 5 replies
  • 3 kudos

B-G431-ESC1 motor profiler connection

Hi, I'm trying to connect B-G431-ESC1 board, with no success. there is always : try to configure the boardI complile and flash a sample project successfully on the board. However still cannot connect motor profiler to make precision tuning of the mot...

Kamil1_0-1766945089159.png
Kamil1 by Associate III
  • 1213 Views
  • 26 replies
  • 0 kudos

Speed PI Gains used in MCSDK

In this documentation, I can find a detailed description of the torque/flux (current) PI controller implementation, but there is no clear explanation of the speed PI controller design or tuning. Could you please explain how the speed PI (KP, KI) is d...

TRUONGGIANG_0-1769756134270.png