cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-SPN5 Installation

dhva1234
Associate II

hello,

I am a student, and for my university project, we are using this stepper motor controller X-NUCLEO-IHM05A1, and I have the STM32NucleoF401RE Microcontroller board to send the command to the motor control. I see there is one middleware package for this motor controller called X-CUBE-SPN5. So, I try to search for this middleware package on STM32CubeIDE, but there is no option regarding it. Now I go to the ST website and I am looking for the .zip file, but there is nothing. I also try to find the proper use case, how can I install, and how can I use but is there any documentation available for that? So can you please provide me this package so I can control the motor easily for my university project, and if possible, so guidance on how i install this middleware package into STM32CubeIDE and how to use this middleware package function for controling the motor.

 

I am waiting for your reply.

 

Thanks in advance

Dhruv

@Peter BENSCH 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @dhva1234,

The package X-CUBE-SPN5 is back online and available to download here:

 X-CUBE-SPN5 - Bipolar stepper motor driver software expansion for STM32Cube - STMicroelectronics

Regards

Cedric

View solution in original post

7 REPLIES 7
STuser2
Senior III

You can install MCSDK 6.4.0 and it will automatically install all the related drivers, i am not sure about your board but generally that is followed.

Hi,

MCSDK is not the solution here. It focuses only on PMSM/BLDC motor with 6-step or FOC algorithm. It does not address the stepper motors.

I am checking internally what can be done.

Regards

Cedric

dhva1234
Associate II

.

Hi Cedric,

Thank you for the clarification. I appreciate you checking internally regarding the stepper motor support.
Looking forward to your update.

Best regards,
Dhru

Hello @dhva1234,

The package X-CUBE-SPN5 is back online and available to download here:

 X-CUBE-SPN5 - Bipolar stepper motor driver software expansion for STM32Cube - STMicroelectronics

Regards

Cedric

Hello @dhva1234,

Did you review the X-CUBE-SPN5 link, and was it what you were looking for?
If yes, could you set @Cedric H's response to "Accept as solution"?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
GMA
ST Employee

Hello @dhva1234,

If the response does not meet your expectations, do not hesitate to open a new thread.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA