STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1781 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4927 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9674 Views
  • 5 replies
  • 3 kudos

Resolved! EVSPIN32G4 Motor Current Sensing

Hello,Here are a few things I need to clarify regarding the EVSPIN32G4 current measurement and the related MCSDK software:Referring to section 5.6.1, 5.6.2 and 5.6.3 of the UM2850, I believe that the topology using three standalone OpAmps presented i...

LPort.2 by Associate
  • 6091 Views
  • 9 replies
  • 2 kudos

Motor Driver Fully Isolated shunt reading

Hello everyone, I am currently working on a fully isolated motor driver using an STM32G474RE. I need to interface the AMC1301differential output to the MCU in a way that ensures accurate measurements. What is the best approach to achieve this? Also i...

Zek_De_1-1778338412280.png Zek_De_0-1778280329003.png Zek_De_0-1778338366696.png
Zek_De by Senior
  • 334 Views
  • 6 replies
  • 1 kudos

ST Motor Control Workbench support for H7A3

Hi All, For the project I am working on we are looking to standardize on the STM32H7A3 processor. I am current looking to setup a project in the ST Motor Control Workbench (v6.4.1) targeting the STM32H7A3.When selecting a board, there are only 2 H7 b...

lee22 by Associate
  • 187 Views
  • 1 replies
  • 0 kudos

Request MCSDK for Linux

Please provide a Linux version of MCSDK. ST already has CubeMX and CubeIDE for Linux and they also run on Java, so I guess it should not be a problem.Or even a better alternative, just provide source code for MCSDK examples in a git repository. It is...

test_dot by Associate
  • 923 Views
  • 2 replies
  • 4 kudos

Resolved! B-G431-ESC1 Hall sensors connection issue

Hello, I am using a B-G431-ESC1 board to power some BLDC motors. I have alrady used it succesfully to spin some 2 pole pairs BLDC using Hall sensors for speed control. I even managed to implement some code to stop the motor at every half rotation of ...

Da3 by Associate II
  • 299 Views
  • 1 replies
  • 0 kudos

STSPING4 VDS protection triggered.

About EVSTSPIN32G4, I started the code generated by MotorControl Workbench 5. Y.3 normally.If you transplant the IIC configuration of the pre drive and enable PWM output, the VDS will report an error.After carefully reading the generated code, it is ...

GWenJ.1 by Associate II
  • 1964 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.