STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1380 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 545 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Can't open workspace anymore after update

Hi everyone,I'm running into a consistent crash with STM32CubeIDE 1.18.1/1.19 right after selecting or creating a workspace,  after upgrading from version 1.13.1. I working on a corporate-managed Windows PC with SentinelOne installed.I attached the l...

SMoeller by Associate
  • 586 Views
  • 0 replies
  • 0 kudos

CubeIDE forcing you to login to ST [...] - Follow up

The original Thread "CubeIDE forcing you to login to ST ...", opened by @JDoe.2 in August 2023 with 37 Kudos for JDoegot shut down (flagged as read-only) today with a last statement by @Amel NASRI which is marked as "Solution". Congratulations ST, no...

CBerg by Senior II
  • 8120 Views
  • 29 replies
  • 44 kudos

Resolved! Configure a GPIO pin as EXTI

Hello, I am trying to build a api in stm32 cube ide with base mcu as nucleo board.i am planning to build a api with input parameters GPIO_PIN,IRQ_HANDLER_FUN.UserAPI_exticf(GPIO_PIN,IRQ_HANDLER_FUNC){}I don't want ot configure gpio as exti in .ioc fi...

Debugging issues with STM32CubeIDE / STM32F030F4Px

I am having debugging issues with STM32CubeIDE. the processor is STM32F030F4Px and I am using a knock off ST-Link V2. It seem that no matter what I configure I get the same error. There also is a check GDB server version error in the IDE window. Open...

DHirs.2 by Associate
  • 5474 Views
  • 5 replies
  • 0 kudos

SPI GPIO control - AFCNTR bit with LL API

When using SPI LL API on STM32H7, we want to use the CFG2[AFCNTR] bit. When “Master Keep IO option”  is used in the IDE, Cube does not generate the LL_SPI_EnableGPIOControl() function call so that the bit remains unset. This has then has to be called...