cancel
Showing results for 
Search instead for 
Did you mean: 

Can't open workspace anymore after update

SMoeller
Associate

Hi everyone,

I'm running into a consistent crash with STM32CubeIDE 1.18.1/1.19 right after selecting or creating a workspace,  after upgrading from version 1.13.1. I working on a corporate-managed Windows PC with SentinelOne installed.

I attached the log file below. Based on what I see, I think it could be a problem with a certificate or proxy settings, maybe some leftovers from the old 1.13 version. We had some proxy changes internally, while I must say... I am the only one with these problem here.

What I’ve tried:

  • Fresh install of CubeIDE (even removed CubeMX)

  • Creating new workspaces with different names and paths

  • Forcing trust store type via .ini and environment variable

  • Disabling Eclipse proxy settings (-Dorg.eclipse.core.net.enableProxies=false)

No luck so far. Has anyone run into this before with Eclipse-based IDEs or corporate security software?

Any help is appreciated!

0 REPLIES 0