STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1318 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 527 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Error while flashing NUCLEO STM32L432KC

Hi,I am getting an error while trying to debug my new NUCLEO STM32L432KC board. I am using the STM32CubeIDE v1.1.0 on MacOSx Mojave. See the attached debug log for the error.Error message from debugger back end:Error finishing flash operationFailed t...

VInox by Associate
  • 963 Views
  • 0 replies
  • 0 kudos

Detect key pressed on keyboard usb

I did usb keyboard on stm32 with cubeide. I can send keys to PC. I modified mouse example code generated by cubeide mx to get keyboard HID.​Is there a way to detect what key was pressed on physical keyboard with stm32?​ I use firs bit of report to se...

oeliks by Senior
  • 968 Views
  • 0 replies
  • 0 kudos

How to add a Cube package to my IDE project

I'm working on a basic project using the B-L475E-IOT01A board. I would like to add the Azure and the SBSFU cube packages to the project, however these don't show up in the IDE under Additional Software. I have the zip files downloaded, is there ...

SBade.1 by Associate II
  • 640 Views
  • 0 replies
  • 0 kudos

Problem regarding sleep mode in CUBE IDE

I have ported my source code from IAR to ST CubeIDE.My IAR code is working fine for Sleep mode.But same code is not working for sleep mode in CubeIDE.While debugging i found that it is not going in Sleep mode .Please suggest how can i proceed to make...

PShar.11 by Associate
  • 895 Views
  • 0 replies
  • 0 kudos

Writing data to internal flash

I have a custom board using a STM32F071VTB processor. I would like to store a small amount of configuration data in flash. The configuration can change during operation so that I need to be able to write to the flash from the executing application ...

open serial port failed? (virtual com port debug)

i used CUBEIDE to config my board's VCP function,but virtual com port always open failed,when the board is running in debug mode.so i used CUBEMX to generate my project again, but this time i generate keil project and everything is ok. so what's the...

SWu.2354 by Associate
  • 1052 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE needs IDE built-in usage examples.

I was used to using the Arduino IDE, and I think it might be easier to use the STM32CubeIDE software if there are usage examples built into the IDE. This makes it convenient to use the IDE without having to copy and paste external code to complement ...

0690X00000BugXcQAJ.png
by Not applicable
  • 1107 Views
  • 3 replies
  • 0 kudos