STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1369 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 539 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeCLT 1.19.0 released

We are pleased to announce that the release 1.19.0 of STM32CubeCLT is available. What is new in 1.19.0: Support for ST Arm Clang toolchainMaintenance of the previous versionUpdated in accordance with STM32CubeIDE v1.19.0 Main fixed issues in 1.19.0: ...

Can't Download STM32CubeIDE

i tried many times to download stm32cube ide but it doesnot give me download link to start downloading , whenever i press latest download and login with my profile and press accept for terms and conditions it gives nothing, its not only for Stm32cube...

Choose different builds for "Run" and "Debug" button

Currently the behaviour of CubeIDE is to always choose the same build configuration for the Run and Debug button.Is there a way to have the two seperated? Most of the time I want to flash the Debug build for debugging and the Release build with stron...

A.D. by Senior
  • 2582 Views
  • 3 replies
  • 2 kudos

STM32CubeIDE on openSUSE Tumbleweed

Hello,I try to get STM32CubeIDE working on openSUSE Tumbleweed. But the application won't start due to some error.The log files I have attached. Does someone have an idea or experience with this OS?

MBabu.3 by Associate II
  • 357 Views
  • 1 replies
  • 0 kudos

custom objcopy command

Is it possible to edit the objcopy command emitted by the Stm32CubeIDEIDE? I need to make some adjustments to keep some RAM addresses from showing up in the hex file. Advice on the internet seems to thing this is easily adjustable in the IDE. However...

Carl_G by Senior III
  • 365 Views
  • 1 replies
  • 0 kudos

Resolved! Build Analyzer issue

Hello,Is there a trick to get the Build Analyzer to produce data every time the code is compiled?   It seems like the only way I can get it to update the window is if I change something in the linker script file and recompile again.   Is there an eas...

matt-crc by Senior III
  • 10317 Views
  • 21 replies
  • 10 kudos