2025-07-23 9:49 AM
Hello,
I try to get STM32CubeIDE working on openSUSE Tumbleweed. But the application won't start due to some error.
The log files I have attached. Does someone have an idea or experience with this OS?
2025-07-30 7:05 AM
Hello @MBabu.3
Unfortunately, STM32CubeIDE is not supported on the openSUSE OS yet. Below are the supported operating systems and architectures for STM32CubeIDE
• Windows® 10 and 11, 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 41
• macOS® 14 (Sonoma), macOS® 15 (Sequoia)
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.