STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1450 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 568 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How can I set STM32CubeIDE in the following way

Preamble: consider I have an STM32F4 Discovery Board.Hi,STM32CubeIDE offers a very good interface and opportunities. However, I am type of a person who wants to actually see each step. So, I want such a configuration that, only the minimum set of re...

YAkse by Associate III
  • 1684 Views
  • 3 replies
  • 0 kudos

I am using STM32CubeIDE with NUCLEO-G474RE. placed a logic to generate Sinewave (50 Hz) from a lookup table of in Timer1 interrupt. I am trying to plot this waveform in SWV data trace timeline.

Most of the time non predicted values coming in graph (very big numbers but actual sine values are unit vectors). My core clock is 170 Mhz,Timer1 period overflow interrupt rate is 10 K Hzintercafe SWD clock is 24000 K HzSerial wire viewer clock is 2...

RKall.1 by Associate II
  • 1172 Views
  • 0 replies
  • 0 kudos

Wrong address in debug mode.(STM32G431)

Hi I am using STM32G431 and last version of CubeIDE.When I am debugging on ADC12 Common resistor, It's address is 0x50000200.The address should be 0x50000300. How can I change that address? Or Can you change it?

khong.1 by Associate
  • 1577 Views
  • 3 replies
  • 0 kudos

STM32CubeIDE won't run in MacOS 10.15 Catalina

Hi everyone!I try to install STM32CubeIDE in my MacBook Air it turns out there is a problem that is caused by macOS Catalina. When I try, it fails with the following error message: "This package is incompatible with this version of macOS. The package...

0690X00000ArcT2QAJ.png
MGine.806 by Associate II
  • 6194 Views
  • 9 replies
  • 2 kudos

Resolved! Does Cube-IDE support launching executables that aren't ELF?

An oldie but still needed, CRC in the last word of the FLASH segment. So I'm fine up until I get to the point when I tell TrueStudio my application is other than an .ELF because at Properties / Run/Debug Settings/ Edit / TrueStudio is hobbled by supp...

n2wx by Senior
  • 7504 Views
  • 16 replies
  • 0 kudos

Enable the UART2 Peripheral Clock

Hello, I am doing a UART example and I need to find the command to Enable the UART2 Peripheral Clock. I have enabled the GPIO clock: __HAL_RCC_GPIOA_CLK_ENABLE(); // stm32f4xx_hal_rcc.hand now I need to enable the UART2 Clock Peripheral. Can anyone ...

JLIND.1 by Associate III
  • 4946 Views
  • 8 replies
  • 0 kudos

FreetRTOS Help

Hello, I am going through a Udemy course on the FreeRTOS. The course does not use the latest version of STM32CubeIDE so I am having some troubles. I am using the Nucleo-F446RE Development kit. I have added the library STM32F4xx_StdPeriph_Driver and t...

JLIND.1 by Associate III
  • 2370 Views
  • 4 replies
  • 0 kudos