STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1372 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 540 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Migration from TrueSTUDIO to STM32CubeIDE, missing icons.

I just migrate a project from TrueSTUDIO to STM32CubeIDE. I am quite disappointed, the compilation and launching of the debug are twice as long. How is it possible ? This does not go in the direction of progress.How to recover the very practical icon...

0693W000000VsrLQAS.png

where is internal register

Hi . first of all is there any complete resource for all feature of stm32cubeIDE?Second of all in keil in debug mode we have a part for internal register of processor which show us the operating mode of processor for example thread or handler mode (a...

0693W000000VoVfQAK.png
M N by Associate II
  • 999 Views
  • 2 replies
  • 0 kudos

How to measure CPU usage using CMSIS FreeRTOS?

Hi! How do I measure CPU usage for every task in CMSIS FreeRTOS?I enabled all run time and task stats gathering related definitions (GENERATE_RUN_TIME_STATS, USE_TRACE_FACILITY and USE_STATS_FORMATTING_FUNCTIONS) in STM32CubeIDE GUI.When I call vTask...

rrnicolay by Associate II
  • 8004 Views
  • 6 replies
  • 0 kudos

Resolved! How to disable breakpoint in hard fault handler?

I'm controlling the temperature of high power heaters in my project. Because ithe product can damage if the heaters stay on too long, I have added code to disable the heaters in the hard fault handler. This way I can be sure that if something goes wr...

luuk by Associate II
  • 2164 Views
  • 2 replies
  • 0 kudos

How can I set STM32CubeIDE in the following way

Preamble: consider I have an STM32F4 Discovery Board.Hi,STM32CubeIDE offers a very good interface and opportunities. However, I am type of a person who wants to actually see each step. So, I want such a configuration that, only the minimum set of re...

YAkse by Associate III
  • 1665 Views
  • 3 replies
  • 0 kudos