cancel
Showing results for 
Search instead for 
Did you mean: 

Avast virus checker tells me that the newly installed STM32CubeIDE is infected (see attached). What should I do?

SQuin.2
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Markus GIRDLAND
ST Employee

I’ve sent the request to the developers to also sign the windows binaries for future releases which they say won’t be a problem for future releases because now the ST-LINK GDB server is built separately from the CubeIDE build, which wasn’t the case previously.

We didn’t sign the windows binaries before because they were just a step in the build process and the signing process needs to be done manually.

For now, I would create an exception to allow the file.

So to summarize: It will be fixed in future releases of CubeIDE.

View solution in original post

2 REPLIES 2
Markus GIRDLAND
ST Employee

I’ve sent the request to the developers to also sign the windows binaries for future releases which they say won’t be a problem for future releases because now the ST-LINK GDB server is built separately from the CubeIDE build, which wasn’t the case previously.

We didn’t sign the windows binaries before because they were just a step in the build process and the signing process needs to be done manually.

For now, I would create an exception to allow the file.

So to summarize: It will be fixed in future releases of CubeIDE.

Thank you for a most comprehensive answer Markus.