STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1537 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 586 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Can I use the vl53l1x sensor API without the expansion shield?

I am new to the STM32 and trying to use the vl53l1x sensor. I found a nice article about importing the sensor as below.https://www.digikey.com/eewiki/display/microcontroller/Adding+the+VL53L1X+Driver+to+an+STM32Cube+ProjectHowever, not only above but...

SAn.2 by Associate
  • 1796 Views
  • 2 replies
  • 0 kudos

Unable to connect with my board

I bought new STM32F303VCT6 Discovery board .I connect it to the laptop with using USB user port of the board just for checking it is working or not , after that I saw window pop-up with readme and something and I ignored that referring to user manual...

NPAND.11 by Associate
  • 1203 Views
  • 2 replies
  • 0 kudos

Custom download location to avoid using SSD drive

I am using STM32CubeIDE. It frequently downloads large files from internet (e.g.; device specific file when you start a new project, updates, etc).The problem is, the files are downloaded to my C drive which is SSD. The download location is "C:\Users...

EKarg.1 by Associate
  • 877 Views
  • 1 replies
  • 0 kudos

Importing project issue for EVAL board

I am trying to import (STSW-SPIN3202-V1.0.0 ) to cube IDE. I get the following errors. Seem to be related to the linker config file. The paths are not correct. How do i fix this issue ? I used the "Import" from existing project and file import option...

0693W000006HUbyQAG.jpg
PKAci.1 by Associate II
  • 644 Views
  • 0 replies
  • 0 kudos