STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1544 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 586 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How run STM32CubeL4 examples with STM32CubeIDE 1.4.0?

Hi,I´d like run the examples of STM32CubeL4 in STMCubeIDE.In the tutorial "UM1860 User manual", page 17 I read that there´s a directory named "\STM32CubeIDE" with the configuation project to use with STM32CubeIDE. But in the zip file I could not find...

Resolved! "Convert to C++" missing on 1.5.1

I am trying to convert a C project to C++. In the previous version, there was a "Convert to C++" option in the properties. I can't find this in 1.5.1. How to convert to C++ in the new version? Just changing the main.c to main.cpp doesn't do it. ...

JGold.2 by Associate II
  • 4403 Views
  • 10 replies
  • 0 kudos

How do I flash using stlink v3 from Cube IDE?

I currently manage to flash my devices direct from CubeIDE using an stlink V2. However the STM32H7 Discovery board I have has a built in ST-link V3. So how do I flash direct from the IDE WITHOUT having to go through the rather tedious process of ru...

0693W000008GS3MQAW.png
RAshworth by Associate II
  • 1502 Views
  • 0 replies
  • 0 kudos

Resolved! BUG: Display issue on 1.5.1 with Mac Big Sur

First, is this the place to post bug reports for STM32CubeIDE? I'm seeing a few minor bugs but I'll start with this one in case this the right place. A bug was introduced either with a recent release of STM32CubeIDE or with Mac Big Sur. It is hard to...

AVoel.1 by Associate III
  • 2590 Views
  • 4 replies
  • 0 kudos

Resolved! Programming 2 projects at once in STM32Cube IDE

I have 2 seperate projects, the bootloader and the end application.What i want to do is program the bootloader code when i program the application (Run as).I dont need debug capabilities for the bootloader, i just want flash locations 0x08000000 – 0x...

sde c.1 by Senior II
  • 3734 Views
  • 2 replies
  • 0 kudos

How to install (add?) middleware to STM32cubeIDE ?

Hi, Many thanks in advance to help me. And sorry if my question is stupid. I tried to add EEPROM emulation to my NUCLEO Dev board (L476RG). I wasn't able to add this middle ware via the cubeIDE. After that I seen that it is for cubeMX, I tried to but...

dodonny by Associate III
  • 8381 Views
  • 9 replies
  • 1 kudos

C++ code STD::COUT Using STM32CubeIDE 1.5.1 targeting STM32FF746 Nucleo results in a compile error. Hope someone can advice how to solve this.

Middleware used: stm32_usb_deviceLib, freetos, fatfs, lwip. Compiler output: arm-none-eabi-g++ "../SenticsLib/DebugHelper.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -D_DEBUG -DSTM32F746xx -DDEBUG -c -I../Core/Inc -I../FATFS/Target -I../F...

schelven by Associate II
  • 1476 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G030K8 Linker-error When I modify the linkerfile for absolute adressing of a variable within the Flash-Memory I get an unexpected Error "FLASH' overflowed by 31912 bytes".

I created a motor control programm for the STM32G030K8 with the MCDSK Software and imported it into the STM32CubeIDE. The programm compiles and works fine on my hardware. When I try to allocate some data on the last 2k Page of the Flash I get an erro...

ASatt.1 by Associate II
  • 2190 Views
  • 3 replies
  • 0 kudos