STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE import from Raisonance Ride7?

Hi,We have some old projects in Ride7, but we want to stop using Ride7 to work on them. It would be nice to use STM32CubeIDE for these projects. Is there any way to import a Ride7 project, or would I have to build up the project in STM32CubeIDE from ...

andyn_ff by Associate II
  • 1746 Views
  • 2 replies
  • 0 kudos

Chinese characters?

Hello I can enter Chinese characters into the C/C++ editor of STM32CubeIDE ?And how to avoid that already written Chinese character will be interpreted in wrong way in new opened files?i.e. in windows, you can set the non standard character set for ...

LaoMa by Associate III
  • 2392 Views
  • 2 replies
  • 1 kudos

How to use STM32CubeIDE to load hex file on target?

I am using an STLINK V3 and STM32CubeIDE V 1.6.0....I would like to load a hex file instead of the debugger .elf file onto the target. I have followed the online steps and created the hex file....Can someone tell me the steps needed to point STM32Cu...

SWenn.1 by Senior III
  • 12277 Views
  • 4 replies
  • 0 kudos

STM32F746G-DISCOVERY, STM32CubeIDE, FLASH

Hello! While writing a program for writing data to FLASH, communication with DISCO is disabled. It cannot be recreated. DISCO is unusable. Can you protect yourself against it? greetingsAndrzej

How to make LwIP work with CMSIS_V2 in CubeIDE?

Hi,I have a Nucleo-F439ZI board and I am trying to make a simple application that echoes back a message on a UDP port.When I generate a project using LwIP raw API, I am able to make that happen with a callback function and a PCB.However, as soon as I...

GFeke.1 by Associate
  • 1786 Views
  • 1 replies
  • 0 kudos