STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Can't get STM32G0B1VE USB device work.

I use STM32CubeIDE1.6.1 to generate USB device (CDC VCP mode) code for STM32G0B1VE. The PC could not recognize the USB. I tried internal HSI48 clock and PLLQ for USB (clock frequency verified by MCO), I pulled up DP through 1.5k resistor by a GPIO af...

Jackle by Associate III
  • 22123 Views
  • 38 replies
  • 0 kudos

st-link gdb debug

I have one project built in SW4STM32. I download 1.7 stm32ide and want to start this project in stm32ide. I complete comply. It looks pretty good, the whole project use FREERTOS and tick time use timer6, when I start my program. my program trigger ha...

yang hong by Associate III
  • 7728 Views
  • 10 replies
  • 0 kudos

Correct way to deactivate SPI in half-duplex/simplex mode

I am trying to change a STM32F4 from slave to master after certain amount of time, send a message as master, and go back to slave. I found out that configuring the SPI as slave_rxonly and enabling the SPI will cause the clock to unexpectedly sent a c...

0693W00000AMIV1QAP.png
FDomi.1 by Associate
  • 4376 Views
  • 5 replies
  • 0 kudos

How to generate fixed length hex file using STM32CUBEIDE ?

I am trying to develop a boot-loader for STM32H7xx micro-controller. For that i need a hex file of my program, i am using STM32CUBEIDE for that but the problem is that my generated hex file length is not same some line is short but i need fixed lengt...

JP_RS by Associate II
  • 1891 Views
  • 2 replies
  • 0 kudos

Resolved! Migration from Atollic True studio to STCUBE IDE

We have converted project which was compiled by Atollic True studio to STCUBE IDE. We got the message "Migration was successful but Manual settings may be required" Application_converter.log shows warning and other messages.Not sure that migration is...

NGopa.2 by Associate
  • 1744 Views
  • 2 replies
  • 0 kudos