JYoon.5
Associate II
since
2021-11-17
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About JYoon.5
Options
Report User
User Activity
Posts
Replies
cubeide debugger Live Expression, unsigned char value is '-', i cant understand.... using nucleo-F207zg
2021-12-27
Is it possible to detect glass walls in general environments (office glass, exterior wall glass,....) using the ? It will be used for autonomous driving platforms. TOF(VL53L5CX)를 사용하여 �?�반�?�?� 환경�?� 유리벽(사무실 통유리, 외벽 통유리,......)�?� �?지가 가능 할까요? �?율주행 플랫�?��? 활용 예정입니다.
2021-11-17
Re: Is it possible to detect glass walls in general environments (office glass, exterior wall glass,....) using the ? It will be used for autonomous driving platforms. TOF(VL53L5CX)를 사용하여 �?�반�?�?� 환경�?� 유리벽(사무실 통유리, 외벽 통유리,......)�?� �?지가 가능 할까요? �?율주행 플랫�?��? 활용 예정입니다.
2021-11-18
it is correct!!!!
Re: Is it possible to detect glass walls in general environments (office glass, exterior wall glass,....) using the ? It will be used for autonomous driving platforms. TOF(VL53L5CX)를 사용하여 �?�반�?�?� 환경�?� 유리벽(사무실 통유리, 외벽 통유리,......)�?� �?지가 가능 할까요? �?율주행 플랫�?��? 활용 예정입니다.
2021-11-18
thanks for reply, i will do test it