STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1550 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

The STM32CubeIDE has a debugger window that lets you look at the SPF (Special Function Registers). Why are the set of GPIO registers not included? I am trying to see if RA2 and RA9 are set up the same. But I do not know how to look at them in the debugger

 This lets me see most registers. Why are the GPIO registers not included?How do I examine their settings? Normally I would print them out, but I am trying to debug the serial port so I cannot print them out to a terminal. Thanks,

0693W00000Nsq6uQAB.png
KiptonM by Lead
  • 4346 Views
  • 5 replies
  • 0 kudos

Remove all SWV data

When I use SWV Statistical Profiling and click the "remove all collected SWV-data" (red cross button), when I restart the program, no SWV data are collected. Is there a way to overcome this behavior without having to terminate / restart the debug ses...

JPerr.2 by Associate III
  • 1822 Views
  • 3 replies
  • 0 kudos

Resolved! Linking new added h and c files to the project

I've created h and c files in Inc and Src folders, I get the following error: "undefined reference to `ILI9341_DrawPixel'*.h file:void ILI9341_DrawPixel(uint16_t x,uint16_t y,uint16_t color);*.c file:while (x >= y) { ILI9341_DrawPixel(X + x, Y + y, ...

ksale.1 by Senior II
  • 2198 Views
  • 4 replies
  • 0 kudos

Are there integration function library to do integration in STM32H745 ? Are there low pass filter functions that can be used for this problem? if yes , How to use the library functions in STM32 IDE?

I am using ST microcontroller STM32H745Xi for Rogowski coil current measurement.we are using Rogowski coil for current measurement. we have to detect the transient current .Due to Rogowski coil signal, amplitude is different (higher) at high frequenc...

RKhel.1 by Associate
  • 956 Views
  • 0 replies
  • 0 kudos

Support for mbedtls/PKCS7 on a Nucleo-F446RE board

Hi, I need to implement certificate verification based on PKCS7. I use STM32CubeIDE build 12015_20220302_0855. I have enabled the MBEDTLS middleware module and I see that some support for mbedTLS is added to the project, but PKCS7 seems to be missing...

NPlöt.1 by Associate II
  • 2835 Views
  • 5 replies
  • 0 kudos

Resolved! How to setup DMA to GPIO transfer using HAL in the CubeIDE?

My goal is to transfer the contents of an integer array (8 bits per value) to 8 GPIO pins.Using the CubeMX perspective in the CubeIDE (latest version) I configured the DMA2 to work with Timer1 in the memory to peripheral mode. I am using the STM32 F4...

Broyildiz by Associate II
  • 19963 Views
  • 11 replies
  • 1 kudos