STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1415 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE

I have a STM32F3DISCOVERY, STM32CubeIDE, Windows11.After writing the program to STM32F3DISCOVERY and turning on the debug and canceling the break, I still have to do a RESET. Is it possible to set STMCubeIDE so that I do not have to RESET?

No rule to make target

I am getting the following error. It was building successfully a short time ago but after I copied a folder to another folder, its giving me the error. If anyone can please help me with this? I shall be very thankful.make: *** No rule to make target ...

0693W00000Sup4hQAB.png
MAwan.1 by Associate
  • 1796 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to enter debug mode

I'm new to ST32 series, I bought a NUCLEO-L476RG and a B-L475E-IOT01A to get started. When I plug in either of these boards, it installs itself as a ST-Dongle and ST-Virtual COM port. When I execute my code it flashes the board, it starts my code but...

Jvan.19 by Associate
  • 6469 Views
  • 8 replies
  • 0 kudos

stm32cube ide build analyzer not working ?

I can't seem to get the build analyzer to show mamory usage in the "memory regions" ?Sometimes it shows, but usually not. What am I doing wrong ? Or what shall I do to get it show the memory usage always ?

MAalt.1 by Associate
  • 8099 Views
  • 2 replies
  • 4 kudos

Resolved! WHAT IS THE static HAL_StatusTypeDef name_funtion()?

I am using an example that i want use in my keil Project. the example is in stm32cubeide with HAL library, i am working in keil with standard peripheral. i want use.I want to change the statement of this function using standard peripheral, I know sta...

jdo by Associate II
  • 2299 Views
  • 4 replies
  • 0 kudos

Cannot debug using RTOS Kernel Awareness

Having an issue trying to view multiple thread contexts with CubeIDE RTOS kernel awareness. The debugger keeps disconnecting when RTOS kernel awareness is enabledNormal debugging using GDB server is function correctly.Upon enabling RTOS Proxy, after ...

0693W00000SumBLQAZ.png
EWill.4 by Associate
  • 2306 Views
  • 0 replies
  • 1 kudos