STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1315 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 526 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32CubeIDE 2.0.0 dark theme

Hello,It's been two years since version 1.14.1 (everything was fine there) – is it really that hard to remove these white scrollbars? It's impossible to use STM32CubeIDE...BR

v20.0.0_2.png
bobval by Associate II
  • 1351 Views
  • 10 replies
  • 4 kudos

Resolved! CubeIDE or CubeMX link to Github to use library

Hello colleagues.My first post here...I have seen somewhere in youtube tha it is possible to provide URL to the specific Github location and use code from there as a library or some sort of included component. It has to be special file in Github serv...

3gger by Associate
  • 412 Views
  • 1 replies
  • 0 kudos

STM32CubeCLT 1.20.0 released

We are pleased to announce that STM32CubeCLT 1.20.0 release is available. What is new in 1.20.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.0.0Update of Clang toolchain version 19.1.6Update of GCC 13.3.rel1Update ...

Aimen1 by ST Employee
  • 1054 Views
  • 0 replies
  • 0 kudos

Unable to start CubeIDE v2.0.0 on Windows 7

I have installed the latest IDE in my windows 7 laptop. The installation was successful. When I open the application, I face the following error: An error has occurred. See the log file ....\configuration\.Log file:!SESSION 2025-11-22 14:02:55.630 --...

GongGing by Associate
  • 909 Views
  • 3 replies
  • 3 kudos

Resolved! Unable to start STM32CubeIDE_2.0.0

Hello,I can not start STM32CubeIDE_2.0.0.I have the following error:D:\ProgramFiles\STMicroelectronics\STM32CubeIDE_2.0.0\STM32CubeIDE;;.C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32-4966r5.dll: La procedure specifiee est introuvableCan't load librar...

MLe M.1 by Associate II
  • 592 Views
  • 5 replies
  • 3 kudos

Resolved! STM32G0 hardfault and signal handler FFFFFFF1

I'm trying to find the cause of a hard fault in my code. The problem repeatedly appears after a few or more minutes after starting the  code, sometimes not at all, sometimes every time at close startup after enabling interrupts, and somethimes after ...

Xme_0-1716273865159.png Xme_2-1716274145362.png
Xme by Associate II
  • 7097 Views
  • 9 replies
  • 3 kudos