STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1569 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 596 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32CubeIDE 1.13.1 problem

Hello, while using 1.13.1 version of STM32CubeIDE on a  STM32H735G-DK board I encountered 5 errors which did not happen while using previous versions.The errors are as follows:Can anyone help with what might cause these errors and how can they be fix...

err.PNG
fzbarati by Associate
  • 2160 Views
  • 3 replies
  • 0 kudos

Resolved! Implementing encryption on the STM32L073RZ board

How can I implement the encryption option on the STM32L073RZ board, is that ok with this „https://www.st.com/en/embedded-software/x-cube-cryptolib.html#get-software" link?What is the best algorithm for my board?  Can you please give the Implementatio...

Whiz by Associate
  • 1337 Views
  • 1 replies
  • 1 kudos

Resolved! Live expression wrong type format

Do someone know how to fix the wrong type format on Live Expression under Debug?The format is uint16_t which "live expression" understand corretly, but shows  signed int.Please, see the picture attached.It was right on old CUBE versions...Regards.

JSILV.2 by Senior
  • 7263 Views
  • 4 replies
  • 2 kudos

Resolved! Why does not accept the MCU name?

On CUBE IDE Target Selector, on choosing NEW MCU the selection box do not accept anymore the MCU's name?The box accept only one letter and jumps to the next box?Like the attached picture.

JSILV.2 by Senior
  • 3012 Views
  • 3 replies
  • 2 kudos

Resolved! STM32CubeIDE problem with callback function

Hi, I have writen simple callback function for handle end of ADC convertion in main.c file. In main.h is declared extern void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc); main.c void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc){adc_Complet...

OM by Associate II
  • 2901 Views
  • 2 replies
  • 0 kudos

command line toolchain plugin install

Our stm32cubeide project 1.13.1 is using 10.3-2021 toolchain. I'm configuring a docker for automated builds. So far the only way I've identified to install the specific toolchain is by running the GUI toolchain manager. Once installed, the build succ...

jemason by Associate
  • 2460 Views
  • 1 replies
  • 0 kudos

STM32H747I-DISCO: testing a simple project

Hi,I have a STM32H747I-DISCO board and I'd like to HW debug a simple CubeMX project. I have CubeMX, CubeIDE all with the latest version. I've generated the code. After the code generation I have two subproject  CM4 and CM7. I can Build both of them. ...

Test User by Associate III
  • 4490 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.