STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 592 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! RTC calibration oputput on STM32H7x with LL driver - Bug report

Hello,I tried to enable in the CubeMX section PB2 as calibration output, but it was not working.The fix is to add a couple of lines after the RTC init:... /** Enable Calibration */ LL_RTC_CAL_SetOutputFreq(RTC, LL_RTC_CALIB_OUTPUT_512HZ); //<-...

MD by Associate II
  • 2134 Views
  • 3 replies
  • 0 kudos

What's cause of HardFault_handler () ?

Hi,During debugging in my code, I enter in the function HardFault_handler (), I know then this error is about the registers but I don't know how interpreter this registers. 

0693W00000AMNcWQAX.png
GPaiv.1 by Associate III
  • 23870 Views
  • 4 replies
  • 1 kudos

STM32WB55 Bluetooth examples problem

Dear ST!We recently bought 2 Nucleo WB55RG boards for Bluetooth host/server purposes. Downloaded the p2p host and server BLE example projects from the STM32Cube_FW_WB_V1.17.0 pack, directly from that repository the applications work flawlessly. I'd l...

s_erno by Associate
  • 1929 Views
  • 2 replies
  • 1 kudos

HAL_I2C_Mem_Read_IT

I'm using the Nucleo-G491RE board, and the STM43G491VET chip. The call to HAL_I2C_Mem_Read_IT works on the chip, but not on the Necleo board. The .ioc is the same for both, but the Nucleo says HAL is busy if you go into the HAL code. Both are using a...

VPICINC by Associate
  • 1161 Views
  • 1 replies
  • 0 kudos

Resolved! How to solve STM32CubeIDE compile error?

After re-install the OS(win10), and install the cube IDE to 1.10, I can't compile pass the project which work well before.Could you kindly show me why and how to solve this questions?Thanks!d:\program files (x86)\st\stm32cubeide_1.10.0\stm32cubeide\p...

0693W00000WJCqAQAX.png
kaka.zhuo by Associate II
  • 8095 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L4 series: Bootloader from system memory

Hi, I'm using an STM32L4P5ZG microcontroller, trying to do a bootloader program. Entering into bootloader mode, exit after a fraction of a second and jump to the main loop. Not staying in the bootloader mode. I tried enabling through software to PH3 ...

Lavanya1_0-1696396826542.png
Lavanya1 by Associate II
  • 3330 Views
  • 2 replies
  • 0 kudos